Other Parts Discussed in Thread: ISO124
We have an application that requires signal isolation and an output that is within 0.02% of the input throughout the range -10.24V to +10.24V. Our current design, using the ISO124 isolation amplifier, accommodates only a typical 0.05% gain error, for which we compensate using zero and span adjustments. However, the new specification requires the specified accuracy with NO adjustments. We have considered a digital solution using an ADC- optoisolator-DAC combination, but still are not sure that we can achieve the required accuracy. Has anyone had success with an ADC/PWM/DAC solution?