This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: Cannot be used, SPI cannot communicate

Part Number: ADS1299

I bought the ADS1299EEGFE-PDK, but accidentally burned the chip, so I re-purchased the ADS1299-4 to replace it, but when I opened the ADS1299ECG-FE Evaluation Software on the computer, the software stayed at the step of reading the register , other operations cannot be performed.
So I bought another ADS1299EEGFE-PDK, and confirmed that the functions are normal. I bought a few more ADS1299-6s to replace them. The phenomenon is still the same, and it still stays in the step of reading the registers, and cannot perform other operations.

I'm sure my soldering is good, what I want to know is, what's the difference between ADS1299-4 and ADS1299-6, why it can't be used normally on ADS1299EEGFE-PDK.
The models I am using are 32A0GVTG4 ADS1299-4 and 33ARL0TG4 ADS1299-6 respectively.

What I want to know is, when using 4-channel, 6-channel or 8-channel ADS1299, what should be paid attention to in software and what should be paid attention to in hardware?