Hello,
My customer has some questions about the LM98640QML-SP settings.
1. When using Sample&Hold Mode as Disabled and CDS Mode as Enable, does the Reference Buffer Power Level of Sample&Hold Register (0x06) affect the performance of CDS Mode?
2. When using Sample&Hold mode as disabled and CDS mode as enabled, can they use Ref Buf PowerDown in the Power Down Control Register as Disable?
3. In the datasheet, the reference signal (OSx+) is recommended to connect ByPass Cap 100nF in CDS mode. When not in use, can they power down the Ref Buffer to reduce current consumption?
Thank you.
JH