Part Number: ADC3424
Could you tell me the serial interface spec of ADC3424?
According to ADC3421-24.pdf P48 Table6,
fSCLK = 20MHz MAX
tDSU = 25ns min
tDH = 25ns min
But, when fSCLK = 20MHz, this clock time (tSCLK) = 50ns,
and if 50% duty, clock high time = 25ns, clock low time = 25ns.
Then, tDSU and tDH can't meet 25ns min.
(Bacause it is impossible to get longer tDSU/tDH than clock high/low time.)
Does this spec indicate we can't operate this interface with 20MHz frequency?
Thank you.