Part Number: DDC2256A
Hi,
Is there a problem with the definition of DDC2256 data manual? (As shown in the figure)
0x10 [5:4] is 2 bits, and the following description is 3 bits.

Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DDC2256A
Hi,
Is there a problem with the definition of DDC2256 data manual? (As shown in the figure)
0x10 [5:4] is 2 bits, and the following description is 3 bits.

Thanks!
Hi,
It seems that you got some older/wrong DS. The bits are 0x10[6:4]
This is an NDA restricted device. To obtain the full DS or for further discussions, please contact us directly following the link on the product folder.
Regards,
Eduardo