Part Number: AFE5801


Hi,
In AFE5801, Is there any provision to use only one channel and disable other channels to avoid the current consumption?
Thank You,
Shilpa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AFE5801


Hi,
In AFE5801, Is there any provision to use only one channel and disable other channels to avoid the current consumption?
Thank You,
Shilpa
Hi Shilpa,
Yes. Use PDN_CHANNEL<7:0> and PDN_LVDS<7:0> to disable the required channels and save power.

Thanks,
Karthik
Hi Shilpa,
You can use the below table from the datasheet for an approximate estimate.

Eq (1): Total power (power up) = Per-channel-power (power-up) * 8+ Common-power (power-up) = 522 mW
Eq (2): Total power (power down) = Per-channel-power (power-down) * 8 + Common-power (power-down) = 8 mW
Eq (3): Assume Common-power is negligible
Then, Total power (1-ch power up + 7-ch power-down) = Per-channel-power (power-up) + Per-channel-power (power-down) * 7 = 73 mW
With some margin, you can assume 75-100 mW for 1-ch power up mode. For more accurate estimation, I recommend to procure AFE5801EVM and conduct these measurements.
Thanks,
Karthik