This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC10065: VREF Pin 6 in a single ended configuration

Part Number: ADC10065

After reviewing the data sheet and the Users guide for the evaluation board it looks to me that the 1.2V VREF in an internal voltage and you don't have to connect it to an external voltage.

I have a board that matches Figure 43 on the Datasheet but not getting the results I expect.

I would have expected

2.2V at Vin+ would give me 1023

0.2V at Vin+ would give me 0

2.2 at Vin+ would give me 512

Thanks

 Dave