Part Number: ADC12D1600RF
Hello,
Can the sampling clock inputs be driven directly using an LVPECL or CML XO?
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC12D1600RF
Hello,
Can the sampling clock inputs be driven directly using an LVPECL or CML XO?
thank you
HI Rajan,
Pg. 59 of the datasheet in section 6.1.2 states: "The ADC12D1x00RF has a differential clock input, CLK+ and CLK-, which must be driven with an ACcoupled, differential clock signal. This provides the level shifting necessary to allow for the clock to be driven with LVDS, PECL, LVPECL, or CML levels. The clock inputs are internally terminated to 100-Ω differential and self-biased."
Regards, Amy
Hi Rajan,
Please define high-power, do you have a certain number of dBm you need?
Are you looking for a stand-alone oscillator, or do you need a clocking chip recommendation?
Or, are you looking for a recommendation for an external signal generator?
Regards, Amy
Amy,
The ADC can accept a differential clock input power from -7 to +7 dBm and I want to clock it near its maximum to maximise performance at high frequency. LVPEC and CML can be considered, but differential sine wave would potentially produce larger amplitude ...
Hi Rajan,
Are you looking for a stand-alone oscillator, or do you need a clocking chip recommendation?
Regards, Amy
Hi Rajan,
Hope you are doing well!
Can you please define high power, in dBm? Vpp?
Thanks,
Rob
Hi Rob,
Hope you are well.
I'm looking for a single-ended, sinewave XO capable of outputting +6 dBm or higher please.
Kind Regards,
Rajan.
Rajan,
Please see VCXO options from Crystek. https://www.crystek.com/home/crystek/default.aspx
Regards, Chase