This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Level Translator requirement

HI,

We have a requirement on 8 channel (3.3V to 1.8V ) direction control level translator for ycbcr bt656 8bit parallel interface.

Can you please suggest the part number which meets the above requirement?

Regards,

Chitharanjan M

  • Hey Chitaranjan,

    Based on this app brief that I found, the upper limit of data rate to be 30MHz. Here is a direct link of all translators will be able to support this speed at this voltage node. Devices denoted with an H in it means that it contains bus-hold inputs that allow any unused inputs to float.

    Please let me know if there are any other system requirements in your application (i.e strict timing specs). 

    Regards,

    Jack