Part Number: TX7332EVM
Hello,
We have just received the instrument TX7332EVM and are planning to run some tests.
Could you please help me with some questions?
Do you know the maximum current and voltage driving capability of the device?
Is the device limited by power dissipation or the current? If I want to test 32 devices each with 100pF at 2MHz, with 60V amplitude voltage for each one. Are we able to drive it if we have a very small duty cycle? Or the hardware is limited to 1.2A cap?
Does 1.2 A correspond to some voltage value? Or we can operate within all the ranges of the maximum voltage value(100V) while still output a maximum 1.2A?
Thank you!
Best,
Yuqi