Part Number: ADS8887
When I provide a 4.7V voltage to the Ui signal using voltage divider resistors and turn on the power switch, the currents for +15V and -15V are relatively high, as measured through R60 and R64. However, there are three cases where the current is not high: 1. When I remove the ADC U1, the current is not high. 2. When I remove the Ui input and leave it floating, then power on, the current is not high. 3. When I power on the circuit first and then apply a 4.7V voltage to Ui, the current is also not high.
I don't understand these phenomena and would appreciate your help in resolving them or providing relevant information.
Thank you very much.