This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8728: DAC8728

Part Number: DAC8728

In our design, we are using DAC8728 chipsets to set Analog outputs.  The issue is, we are not able to get the output range of -10V to +10V.

Applied voltage details for DAC8728 are : AVDD = +15V, AVSS = -15V, DVDD = +3.3V, IOVDD = +3.3V, REF : +5V, LDAC = 0V, USB/RTC = +3.3V, RST SEL : +3.3V

DAC OFFSET value = 0x999A (default)

 DAC offset Voltage  on pin 12 :  +3.8V

When DAC set value is 0x0000, Measured voltage at DAC Outx : +5.628V

                   Set Value is 0x7FFF, measured voltage is +6.423V

                    Set Value is 0x8000, measured voltage is -14.967V

                  Set Value is 0xFFFF, measured voltage is +5.628V

What should we do to achieve the output range of -10V to +10V? what is value to get 0V at DAC output?

Kindly guide us to resolve the issue.