Part Number: ADC3662
Dear all,
We are designing a board with the ADC3662 configured to use the internal DDC feature with complex decimation.
To simplify the design, we are considering to generate the DCLKIN clock with the FPGA internal PLL.
This clock is used only for the LVDS serial interface and not for the acquisition.
The FPGA is a Xilinx Spartan 7, and the Clock wizard is estimating the PLL output jitter to be greater than 300ps pk-pk.
The maximum jitter for this clock is 50ps in the datasheet, not specifying if it is RMS or pk-pk.
Are there any problems in a similar configuration?
What would happen if the jitter on DCLKIN is too high?
Thanks and best regards
Antonio Climaco