Other Parts Discussed in Thread: ADS1675, OPA211
We are placing multiple ADC1675s on a baord, what is Ivref. We are planning to use the REF5030
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Robert,
The total reference input current when operating with a 32MHz clock is 10.5mA. This is a combination of an equivalent 400ohm DC load, as well as an additional switched-capacitor load. In order to get datasheet performance from the ADC, you will need to include a reference buffer placed as close as possible to each ADS1675 in your system. I suggest using the OPA211 circuit for each ADS1675 with a single REF5030, as shown in Figure 53 of the datasheet.

Regards,
Keith Nicholas
Precision ADC Applications