Part Number: DAC8740H
Hi team,
I received several questions about DAC8740H's carrier detection. Please support.
1) Is the starting point for carrier detection ON the first point where the MOD_IN voltage exceeds the 80-120mVpp threshold?
2) What is the starting point for carrier detection OFF? I cannot understand it bacause it's AC signal so, the voltage swing crosses the threshold voltage every cycle.
3) The maximum CD output delay is "6 Bit-times". Is it 5ms because the UART is 1200 baud rate?(1/1200 * 6 = 5ms)
4) Why the unit of "detect on" is Bit-times but unit of "detect off" is ms?
Best Regards,