Other Parts Discussed in Thread: ADS127L11
Hi,
I'm interested to hear what TI recommend as replacement for ADS1210? I have seen the Obsolete PCN for the ADS1210(TI Number PDN# 20220830000.3) and the two recommended parts there. But I was wondering if it exist anything else that TI recommends that could be evaluated with better 50 and 60 Hz filter rejection. On our design the digital voltages is 5V, analog voltages 5V, analog input is between 0-5V(Ain_neg connected to 0V), External 2,5V ref, SPI, /DSYNC, /DRDY is used. I would like to change as little as possible around the part. Is is possible to have direct phone contact?