Part Number: ADS7950
What is the REFP pin max current draw? Have an application with one source driving multiple ADC chips. Would be nice the info is in datasheet.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS7950
What is the REFP pin max current draw? Have an application with one source driving multiple ADC chips. Would be nice the info is in datasheet.
Hi Xiaoping,
Welcome to our e2e forum! If you look at the reference input resistance on page 13, you can assume ~25uA of current would come from the reference source while the device is converting. How many ADC's do you plan to use? Will they all be sampling in parallel or in a sequential manor?
Thanks Tom!
There will be 8 sampling in sync. The source can easily provide 0.2mA but not sure about 80uF.