This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC63204EVM: Direct SPI communication

Part Number: DAC63204EVM
Other Parts Discussed in Thread: DAC63204

Hello,

The DAC63204EVM works properly with the USB interface in SPI mode.

The next step is to communicate directly with a microcontroller in using the SPI lines SDI, SCLK and SYNC connected to a demo board.

All the jumpers of the DAC63204EVM have been removed and the DAC63204 is power supplied with the VDD.

Unfornutally, the communication SPI does not seem to work. The DAC output does not change even with the same configuration used in USB mode.

Is there other hardware modification of the DAC63204EVM than removed the jumpers to establish a SPI communication with a microcontroller?

Thank you.