Other Parts Discussed in Thread: ADS8689
Hello team,
I have a question about ADS8866. Could you please help me with the answer?
Currently, there are customers who want to use products with Ads8866 at high temperatures.
The operating temperature of Ads8866 is stated to be up to 85 degrees, but actual testing in that environment shows that the case temperature of Ads8866 remains above 90 degrees.
Temperatures of up to 105 degrees have been seen in some cases.
Some reduction in accuracy at high temperatures can be tolerated, but serious problems such as failure should not occur. Therefore, I would like to inquire as follows.
1) For other products, Junction or Case temperature specifications are displayed, but Ads8866 is not displayed. Please tell me the Tj or Tc temperature of Ads8866.

2) Is there a product that is pin-to-pin with Ads8866 and can operate at high temperatures?
Best Regards,
Hongseok