Hello,
I am using the DAC60501, Attach is the SPI signals where the power-up (VDD=3.3V) is the trigger hence the signal in yellow.
I first tried to write the GAIN register and divide the reference by 2 (1.25V) and everything seems to work fine.
When I am setting up to divide by 1 (hence 2.5V), the DAC output is zero volts regardless of the DAC-DATA I am sending.
I have also tried to send a soft-reset first but it did not seem to change anything.
My clock signal is around 6kHz.
Please advice,
-Tal