This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7057: ADS7057 - Error in SPI waveform signal levels

Part Number: ADS7057


Hi,

I am using ADS7057 in one of my design. While using the ADC i am getting erroneous signal levels in the SDO pin of the ADC. I am attaching herewith a photo of the CRO waveform. In this the yellow signal is SDO, blue is the SCLK and the red is CS signal. The SPI clock is supplied by a custom SPI core and is given as two sets of 9 clock cycles while keeping the CS signal low

.

As you can see the SDO line is not stable at logic 1 or 0. I am using  2.5V Vref and 3.3V as DVDD. The SPI clock is 20MHz

Regards,

    Varun M J