This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ3200EVM: What is the step size for ramp test mode ?

Part Number: ADC12DJ3200EVM


Hello Experts,

I am using ADC12DJ3200EVM with KCU105. In ramp test mode I am getting the values are 1, 2057, 4113, 6169, and so on. So, could you confirm the test pattern. 

JMODE = 10

Device clock = 1250 MHz

Refclk = 78.125 MHz

Sysref = 4.8828125 MHz

K = 16