Other Parts Discussed in Thread: ADS7028, ADS8528
Dear!
I am looking for an ADC solution
I need to measure the differential voltage of 8 pairs of signal
The voltage range is -12V to +12V
I need the ADC chip to work independently with the MCU.
The ADC chip measures all channels and updates the converted data in the buffer, the MCU will read out the data when the system needs it.
Please help to suggest suitable part numbers
Thanks and Best Regards
Ryder