Part Number: ADS131A04
Other Parts Discussed in Thread: ADS131B04-Q1
Dear TI team,
i am missing a min/max specification of the differential input impedance Zin. Only the typical value (130 kOhm @ fMOD = 4.096 MHz) is specified. Can You provide such a min/max specification? I would even accept a large deviation from the typical value, as long as the limits are known.
Background:
I am using this ADC with passive RC filtering in front of the analog inputs AINxP and AINxN in a ratiometric configuration. The dominating gain error is therefore the attenuation of the voltage divider consisting of series filter resistor and ADC input impedance Zin. Since i can calculate this voltage divider, i can compensate the typical gain error. What i cannot compensate is the gain error deviation from the typical value, due to the unknown tolerance of the ADC input impedance Zin. Therefore i would like to calculate the maximum expected deviation from typical, to check, if my system still meets my accurracy requirements.
Thanks and best regards,
Stefan