Part Number: ADS8688A
Hi,
I would like to have information regarding the type of memory used in the ADC ADS8688A to store configurations parameters inside the component.
Our project is in the aeronautic field and we would like to avoid a SRAM technology regarding SEU issues.
Please can you tell me which type of memory (SRAM, flash..) is used to store parameters configurations inside the component registers memory?
Please find below my requirements if you can find an equivalent if necessary :
- 6 / 8 channels
- Acquisition / conversion time : 10ms max to read all the channel
- Sampling rate :250kSps
- ADC hardware configuration (preference)
thanks in advance