Hello. I'm trying to understand the best way to use RLD feature. I have the following connections: (LA -> IN1P); (LL -> IN2P); (RA -> IN1N and IN2N); (RL -> RLDIN and RLDOUT and RLDINV (via C and R)).
As far as I understand, RLD feature is configured using register RLD_SENSP and RLD_SENSN. Shall I enable bits for IN1P, IN2P, IN1N for this configuration? I guess it would be a mistake to enable four bits (IN1P, IN2P, IN1N, IN2N) doubling RA contribution?
I also have V1..V6 connected to IN3P...IN8P. IN1N...IN8N are connected to WCT. Does it make sense to enable corresponding RLD_SENSP bits or it's not useful?
Also as far as I understand, RLD works best when all electrodes have good contact with skin. Shall I use lead-off detection feature for those electrodes and adjust RLD_SENSP/RLD_SENSN accordingly on the fly (enabling them only if electrode is not off)?