Other Parts Discussed in Thread: ADS8555
HI Sir
The ADS8556 will freeze in random during the ADC reading
but ADS8555 No any issue in the same circuit, may I know the diff inter?
thans
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alex,
The only difference between the ADS8555 and ADS8556 ADCs is the partial power-down mode which is available on the ADS8556, others are same including the pinout and timing for operation. Also, both of devices offer the data rate up to 630kSPS in Parallel mode or 450kSPS in Serial mode.
Best regards,
Dale
Hi Alex,
If you do not want to use the partial power-down mode, you can directly use ADS8555 that's is pin-pin compatible with ADS8556.
Regards,
Dale