Hello!
I'm using the ADS1158 for measuring some analog values, however I see that frequently the measurements will be completely wrong. I have seen this issue on 3 boards now and I believe I traced the issue down to the fact that AinCom is not a steady GND as expected from our schematics. The GND going into the GND selector MUX is about ~0V, however I see that the AinCom pin seems to have a pulse every few ms, which would explain why the measurements are incorrect.


I disconnected most circuitry from this pin(U26), and still see the pulses so I'm pretty sure they are coming from the ADC. I checked the MuxOutN in comparision to AinCom and see that the AinCom pulse is seen, as well as some other signals which I am unable to explain. This ADC is run differentially with all measurements referenced to AinCom so I don't see how there can be any other pulses outside of those seen on AinCom. My assumption is the ADC internal mux has been damaged, however I am unsure what might cause this issue as I've seen this happen on 3 boards already. Does the issue require me to replace the ADC, or is there some other reason AinCom could be pulsing like this? Any help/info is apprecaited!
MuxOutN(Blue) vs AinCom(Yellow)