Hello all,
I am attempting to generate an analog 5-V sine voltage ([-2.5V;+2.5V]) using the DAC9881, but our home-made board yields the signal as in the figure below :

(this is an Excel curve based on data captured on an oscilloscope).
It is a sine wave over one period, but as you can see, it goes abruptly from to +2.5V to -2.5V or from -2.5V to +2.5V several times.
We are pretty sure the code is correct because the same code works when using the DAC9881 Evaluation Module.
Below, the schematics :

I have read the DAC9881 datasheet, and I have noticed a couple of points :
- the same voltage (V5.5 here) is applied to IOVDD and AVDD pins. Is it a problem ? Should AVDD be settled before powering IOVDD ?
- the /LDAC pin is always connected to GND. Is it a problem ?
- The force and sense pins are tied to the same voltage ( (VREFH-F/VREFH-S tied to 5Vref and VREFL-F/VRFEL-S to GNDB). Is it ok ?
Which one of these points would you investigate first ?
Thank you in advance,
Philippe