Other Parts Discussed in Thread: AMC3336
Due to the absolute maximum ratings of this product, the input voltage range of the INP and INN pins is HGND-6[V]~HLDO_OUT+0.5[V].
If voltage is applied between the INP and INN pins before the AMC3336 is powered on, will the components be damaged?
On page 20 of the data sheet, it is stated that the ESD guidelines will be turned on if the absolute maximum rating input range is exceeded.
In this case, is it correct to understand that there will be no damage to the components even if the input range of the absolute maximum ratings is exceeded as long as the current limit other than ESD is below?