Part Number: ADS124S08EVM
Other Parts Discussed in Thread: ADS124S08
Hello, TI forums.
I am attempting to set up the aforementioned part to test if this A/D is what my company needs. I want to use the Eval board to measure a 4-pin RTD, and have said RTD (well, decade box simulator) hooked up in accordance to the user's guide. My next attempt was to try and run the 4-pin RTD pre-defined script, but that is causing trouble. I've attached the script I'm running to this post. Whenever I run it, The command line says "Unrecognized command: pause" and then "Client went away", at which point I can't seem to do anything else. If I try to reset and then rerun the script, nothing happens, and if I step through, the program will act like it's stepping through, but nothing actually changes.
I've tried manually sending all the register writes using the register map, and that does seem to work, but I don't know how to send a start command this way. If anyone can help tell me what I'm doing wrong, I would greatly appreciate it.