Part Number: ADS5294
Hi team,
Here is a question one of our customers is experiencing, could you please provide some troubleshooting suggestions?
He's trying to use 16bits outputs with decimation enabled, but the output results (captured with vivado ILA) are NOT correct. Before doing this, he has already tested 16bits output without enabling decimation and got correct 16bits results.
The sampling rate is 78MHz ( driven by a differential clock), and ADS5294 is configured to use 1-wire LVDS outputs. The frequency of the input signal is less than 1MHz.
The relevant registers are configured as follows:
0X2E ~ 0X35 <= 0b0000_0001_0001_0001
0X38 <= 0b10
0XD1 <= 0X0140
and 0X46 is configured as
0X46 <= 0b1000_1000_0000_1000
And he also tried to lower the frequency of the input clock to avoid possible timing issues, but the problem still exists.
Best Regards,
Amy