Other Parts Discussed in Thread: OPA335, ADS124S08
I have a photodiode sensor that gives a min-max output between 0.134 mV and 178 mV. I will amplify the output mV of this sensor using OPA335 and then give it to the ADS1248 ADC. The digital data from the ADC will be connected to the STM32F030x processor.
My questions are;
1. Are my steps correct?
2. Are the analog input-output voltages of the integrations I use suitable for each other?
3. Do I need to use another Buffer amplifier after the OPA335 Amplifier? If necessary, which one do you recommend to use?
4. How will I adjust the gain of the amplifiers and ADC I use?
Best Regards,