Part Number: ADS1258
I have configured the circuit as shown below. Are there any problems?
Please help. In particular, since this is my first time using an ADC with a mux part, I am not sure if it is right to add a buffer like that.
The customer's requirements are
V: +1V to -1V
Input qty: 8Differential or 16Single-end
It was composed based on .