Part Number: AFE5809

Hi team.
if I unsoldered the bypass capacitor in AFE5809 INM pin,is there any affects?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AFE5809

Hi team.
if I unsoldered the bypass capacitor in AFE5809 INM pin,is there any affects?
Hi,
Removing capacitor on INM pin is not advisable as it can lead to oscillations in the LNA block.
Regards,
Shabbir
Hi Shabbir,
is the oscillations caused by the invert input pin floating? but if we connect it to the GND, is this issue can be resolved?
Hi
for the LNA ,I didn't see the feedback resistor. is this res integrated into the LNA?
Hi,
Yes oscillation will be due to INM being floating.
No we cant connect INM to ground since it will cause large DC current and functional failure.
Regards,
Shabbir
Yes the resistor setting the LNA gain and also active termination resistor is integrated in the LNA.
Regards,
Shabbir