Part Number: ADS54J60EVM
Other Parts Discussed in Thread: LMK04828
Hi everyone,
We are facing a strange issue with our ADS54J60EVM FMC ADC. While sampling our input signal that varies from 20mVpp up to 1.9Vpp (the maximum swing that should in theory give us the full scale of the ADC) we are seeing at roughly 50% of the time DC bias/offset.
Please refer to the FFT spectra below. In the "problematic" one we can clearly see that the SNR diminishes due to the DC offset while the other one shows normal operation.
As we want to extract the frequency content from the 10MHz - 120MHz range, this is very problematic and difficult to resolve in processing.
The input signal normally does not feature a DC content (if any, it may be at max 10mV). Even if it had a DC content though, shouldn't the passive balun cut it out?
Could this behavior be a due to a malfunction of the DC offset correction block? We have not disabled it, so it should be enabled by default.
We are also seeing interleaving spurs, even if we only give a stable 80MHz input RF frequency. We do not know if this can be avoided.
What do we have to do? Do we have have to use a high pass filter to cut off the DC content completely? Do we have to use a low pass filter to cut above 120MHz? Do we have to use an SMA DC blocking capacitor? We are still trying to figure out if this should be expected or not.