Part Number: AFE58JD28
Hi ,
I iam using AFE58JD28 with TGC mode:
| LNA(dB) | DIG_TGC_ATTENUATION(dB) | PGA(dB) |
| 15 | 24 | 18 |
CLAMP LEVEL= 2.24Vpp
LPF_PROG = 20 MHz
LNA_HPF_PROG = 100KHZ
with input signl of :650KHZ pulse (30 pulses), unfortunately the max ADC data that i get at full sacle is ~26k bins and not 32768 [(2^16)/2].
what can i do to have full sacle of the ADC?
Thanks ,
Nadav