Part Number: DAC80502
Other Parts Discussed in Thread: DAC80504,
Dear Specialists,
My customer is considering DAC80504 and has questions.
I would be grateful if you could advise.
---
DAC80502 datasheet describes offset error and zero code error.
Could you please advise regarding two specs in detail.
(1) Zero code error is considered to be the value of analog output voltage when digital code 0000 is input. Is it correct ?
(2) Offset error is the difference between the ideal value of the output when the digital code is input. Is it correct ?
(3) I don't understand the difference between zero code error and offset error.
Is it necessary to add zero code error and offset error?
For DAC80502,
Offset error is -1.5mVmin 0.5mVtyp 1.5mVmax
Zero code error is -1.5mVmin 0.5mVtyp 1.5mVmax
When entering zero code
Is the error maximum -3mVmin 3mVmax?
(4) The minimum Zero code error and offset error are negative voltages, -1.5mV each.
The output voltage range (Vo) is minimum 0V. It cannot output negative voltage, but what will happen to the actual output?
---
I appreciate your great help in advance.
Best regards,
Shinichi