Part Number: ADC09QJ1300
Hello,
The clock of ADC09QJ1300 is 100Mhz, and SYSREF=7.8125Mhz, the GLBLCLK and REFCLK of FPGA are 125Mhz, SYSREF is 7.8125Mhz.
When used the test mode, he found that JESD204BIP core output messy code.
This is configuration code of ARM core, please help to check:
#include "xparameters.h"
#include "sleep.h"
#include "xgpio.h"
#include "xil_io.h"
#include "xil_types.h"
//#include <stdio.h>
//#include <stdlib.h>
/* // spi的地址和数据
6'h00: rdata = { 31'b0 , spi_busy };
6'h01: rdata = { 8'b0 , spi_wr_data };
6'h02: rdata = { 24'b0 , spi_rd_data };
*/
XGpio LMK_CFG;
#define LMK_BASE_ADDR 0x44A10000
#define ADC_BASE_ADDR 0x44A00000
#define R_JESD_BADDR 0x44A20000
u32 LMK_DATA[136] = {
0x000090, 0x000010, 0x000200, 0x000306, 0x0004D0, 0x00055B, 0x000600, 0x000C51,
0x000D04, 0x01001E, 0x010155, 0x010255, 0x010300, 0x010422, 0x010500, 0x0106F0,
0x010755, 0x01081E, 0x010955, 0x010A55, 0x010B00, 0x010C22, 0x010D00, 0x010EF0,
0x010F55, 0x011018, 0x011155, 0x011255, 0x011300, 0x011402, 0x011500, 0x0116F1,
0x011705, 0x011818, 0x011955, 0x011A55, 0x011B00, 0x011C02, 0x011D00, 0x011EF1,
0x011F05, 0x01200C, 0x012155, 0x012255, 0x012300, 0x012402, 0x012500, 0x0126F1,
0x012705, 0x01280C, 0x012955, 0x012A55, 0x012B00, 0x012C02, 0x012D00, 0x012EF1,
0x012F05, 0x013006, 0x013155, 0x013255, 0x013300, 0x013422, 0x013500, 0x0136F0,
0x013750, 0x013825, 0x013903, 0x013A01, 0x013B80, 0x013C00, 0x013D08, 0x013E00,
0x013F02, 0x014081, 0x014100, 0x014200, 0x014310, 0x0144FF, 0x01457F, 0x014619,
0x014713, 0x014802, 0x014942, 0x014A33, 0x014B16, 0x014C00, 0x014D00, 0x014EC0,
0x014F7F, 0x015003, 0x015102, 0x015200, 0x015300, 0x015473, 0x015500, 0x01560A,
0x015700, 0x015896, 0x015900, 0x015A01, 0x015BD4, 0x015C20, 0x015D00, 0x015E00,
0x015F0B, 0x016000, 0x016105, 0x016244, 0x016300, 0x016400, 0x01650C, 0x0171AA,
0x017202, 0x017C15, 0x017D33, 0x016600, 0x016700, 0x016896, 0x016959, 0x016A20,
0x016B00, 0x016C00, 0x016D00, 0x016E13, 0x017300, 0x018200, 0x018300, 0x018400,
0x018500, 0x018800, 0x018900, 0x018A00, 0x018B00, 0x1FFD00, 0x1FFE00, 0x1FFF53
};
u32 DAC_CFG_DATA[102] = {
0x000018, 0x010003, 0x022002, 0x03A300, 0x040000, 0x05FF03, 0x06FFFF, 0x073100,
0x080000, 0x090000, 0x0A0000, 0x0B0000, 0x0C0400, 0x0D0400, 0x0E0400, 0x0F0400,
0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000,
0x180000, 0x190000, 0x1A0020, 0x1B0000, 0x1E9999, 0x1F9980, 0x208008, 0x221B1B,
0x2301FF, 0x240020, 0x252000, 0x260000, 0x2D0001, 0x2EFFFF, 0x2F0004, 0x300000,
0x311000, 0x320000, 0x330000, 0x340000, 0x3B0800, 0x3C0028, 0x3D0088, 0x3E0108,
0x3F0000, 0x461882, 0x4701C8, 0x483143, 0x490000, 0x4AFF01, 0x4B1200, 0x4C1307,
0x4D0300, 0x4E0F4F, 0x4F1C61, 0x500000, 0x5100DC, 0x5200FF, 0x530000, 0x5400FC,
0x5500FF, 0x560000, 0x5700FF, 0x5800FF, 0x590000, 0x5A00FF, 0x5B00FF, 0x5C1133,
0x5E0000, 0x5F3210, 0x605764, 0x610211, 0x640001, 0x650001, 0x660001, 0x670001,
0x687709, 0x690000, 0x6A0000, 0x6BBD07, 0x6C0007, 0x6D0090, 0x6E0000, 0x6F0000,
0x700000, 0x710000, 0x720000, 0x730000, 0x740000, 0x750000, 0x760000, 0x770000,
0x780000, 0x790000, 0x7A0000, 0x7B0000, 0x7C0000, 0x7D0000
};
u32 Xil_SPI( u32 spi_addr, u32 dev_raddr){
u32 rd_state = 0;
u32 rd_data = 0;
Xil_Out32(spi_addr + 0x04 , dev_raddr); //写入读取数据的命令
do{
rd_state = Xil_In32(spi_addr + 0x0); //读取忙状态
}while(rd_state == 0x1);
rd_data = Xil_In32(spi_addr + 0x8); //读取读出数据
//usleep(1);
return rd_data;
}
int DAC_INIT(void){
}
int ADC_INIT(void){
u32 Xil_Rdata = 0;
Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x800C00); //读取FPGAVID
Xil_SPI(ADC_BASE_ADDR , 0x0000B0); //AD芯片复位,等待750ns,地址0x00,默认数据0x30
usleep(1000);
//do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x820800); }while(Xil_Rdata == 0x0); //读取cpll锁定状态
do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x827000); }while(Xil_Rdata == 0x0); //读取init状态,直到返回1,在继续
//Xil_SPI(ADC_BASE_ADDR , 0x002B05); //设置参考时钟消抖
Xil_SPI(ADC_BASE_ADDR , 0x002A03);
Xil_SPI(ADC_BASE_ADDR , 0x0029B0);
Xil_SPI(ADC_BASE_ADDR , 0x003F4A); //向vco_bias中写入0x4a来设置vco的偏置
Xil_SPI(ADC_BASE_ADDR , 0x005881); //调整调整PLL输入管脚设置为管脚模式或者SPI模式,以及输入模式设置。
Xil_SPI(ADC_BASE_ADDR , 0x005C01); //编程cpll_reset置1到复位以继续cpll编程
//Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x803F00);
Xil_SPI(ADC_BASE_ADDR , 0x003D05); //设置pll_p_div,pll_v_div,目前要求是1000M,根据手册可知,需要的p*v=8,在这里设置成p=2,v=4
Xil_SPI(ADC_BASE_ADDR , 0x003E0A); //设置pll_n_div 公式为:采样率 = N * Fref,因为在SE_CLK口输入的频率为100MHZ,则需要写入十进制的10,即16进制的0A,达到1000M频率 //***********************************
Xil_SPI(ADC_BASE_ADDR , 0x005D41); //设置vco_cal_en到1以启动vco校准
Xil_SPI(ADC_BASE_ADDR , 0x005C00); //设置将cpll设置到0以校准和启动vco及启动cpll
Xil_SPI(ADC_BASE_ADDR , 0x005781); //TRIGOUT输出控制
Xil_SPI(ADC_BASE_ADDR , 0x002B15);
usleep(1000);
do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x805E00); }while(Xil_Rdata == 0x0); //读取vco校准状态直到校准完成
//GET_BIT();
//do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x820800); }while(Xil_Rdata == 0x0); //读取CPLL校准状态直到校准完成(读到1)
do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x820800); }while((Xil_Rdata << 31) != 0x80000000); //读取CPLL校准状态直到校准完成(读到1)
Xil_SPI(ADC_BASE_ADDR , 0x020000); //关闭JESD204接口的状态机,以允许更改设置
Xil_SPI(ADC_BASE_ADDR , 0x006100); //关闭校准状态机以允许设置
//Xil_SPI(ADC_BASE_ADDR , 0x003746); //设置低功率模式1寄存器,设置1G及以内的低功率
//Xil_SPI(ADC_BASE_ADDR , 0x029A06); //设置低功率模式2寄存器,设置1G及以内的低功率
//Xil_SPI(ADC_BASE_ADDR , 0x029B00); //设置低功率模式3寄存器,设置1G及以内的低功率
//Xil_SPI(ADC_BASE_ADDR , 0x029C14); //设置低功率模式4寄存器,设置1G及以内的低功率
Xil_SPI(ADC_BASE_ADDR , 0x020109); //设置JMODE,选定的输出模式为JMODE1
Xil_SPI(ADC_BASE_ADDR , 0x02021f); //设置KM1寄存器,目前的值为默认的十进制的31,即十六进制的1F
Xil_SPI(ADC_BASE_ADDR , 0x020401); //选择同步信号是单端还是查分输入,此处选择默认单端
Xil_SPI(ADC_BASE_ADDR , 0x020505);
//Xil_SPI(ADC_BASE_ADDR , 0x006201); //设置默认前景校准
//Xil_SPI(ADC_BASE_ADDR , 0x006501); //设置默认偏移参考值
//Xil_SPI(ADC_BASE_ADDR , 0x005781); //TRIGOUT输出控制
Xil_SPI(ADC_BASE_ADDR , 0x02130f); //启动超量程显示
Xil_SPI(ADC_BASE_ADDR , 0x006101); //启动校准状态机
Xil_SPI(ADC_BASE_ADDR , 0x020001); //启动jesd204的状态机
Xil_SPI(ADC_BASE_ADDR , 0x006C00); //拉低启动前景校准器的命令
Xil_SPI(ADC_BASE_ADDR , 0x006C01); //拉高启动前景校准器的命令
do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x806A00); }while(Xil_Rdata == 0x0); //读取前景校准状态直到校准完成
return 0;
}
int RD_JESD_INIT(void){
u32 Xil_Rdata = 0;
Xil_Out32(R_JESD_BADDR + 0x08 , 0x01); //启动ILA
Xil_Out32(R_JESD_BADDR + 0x0C , 0x00); //不加扰码
Xil_Out32(R_JESD_BADDR + 0x10 , 0x01); //掉链后自动重连
Xil_Out32(R_JESD_BADDR + 0x18 , 0x00); //测试模式选择普通模式
Xil_Out32(R_JESD_BADDR + 0x20 , 0x00); //设置F = 1
Xil_Out32(R_JESD_BADDR + 0x24 , 0x1f); //设置K =32
Xil_Out32(R_JESD_BADDR + 0x28 , 0xff); //设置全通道启动
Xil_Out32(R_JESD_BADDR + 0x2C , 0x01); //设置子类1
//Xil_Out32(R_JESD_BADDR + 0x2C , 0x00); //设置子类0
Xil_Out32(R_JESD_BADDR + 0x30 , 0xfff); //设置RX缓冲延时
Xil_Out32(R_JESD_BADDR + 0x34 , 0x00); //关闭错误计数,启动sync报错
Xil_Out32(R_JESD_BADDR + 0x04 , 0x00010001); //启动复位信号
do{ Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x04); }while( Xil_Rdata != 0x00010000 );//等待RX的reset拉低(reset完成)
do{ Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x38); }while( Xil_Rdata != 0x00010001 );//等待RX获得sync和连接
/*
while(1){
usleep(1);
//Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x04); //复位状态
Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x38); //sync状态
Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x1C); //链接错误报警
//Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x30);
Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x34); //错误报告
Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x824);
}
*/
return 0;
}
int LMK_INIT(void){
int status;
u32 Xil_Rdata = 0;
/*
do{ status = XGpio_Initialize(&LMK_CFG , XPAR_GPIO_0_DEVICE_ID ); }while( status != 0 ); //设置使能初始化
XGpio_DiscreteWrite(&LMK_CFG, 1, 0x0);
usleep(500);
XGpio_DiscreteWrite(&LMK_CFG, 1, 0x1);
usleep(1000);*/
do{ status = XGpio_Initialize(&LMK_CFG , XPAR_GPIO_0_DEVICE_ID ); }while( status != 0 ); //设置使能初始化
XGpio_DiscreteWrite(&LMK_CFG, 1, 0x1);
Xil_SPI(LMK_BASE_ADDR , 0x000090);
usleep(1000);
Xil_SPI(LMK_BASE_ADDR , 0x000010);
usleep(1000);
XGpio_DiscreteWrite(&LMK_CFG, 1, 0x0);
Xil_SPI(LMK_BASE_ADDR , 0x014A33);
usleep(1000);
Xil_Rdata = Xil_SPI(LMK_BASE_ADDR , 0x800400); //读取PROD ID MSB
Xil_Rdata = Xil_SPI(LMK_BASE_ADDR , 0x800500); //读取PROD ID LSB
int i = 0;
for( i = 2; i <= 136; i++){
Xil_SPI(LMK_BASE_ADDR , LMK_DATA[i]);
usleep(1);
}
return 0;
}
int main(void) {
//u32 Xil_Rdata = 0;
usleep(1000);
LMK_INIT();
usleep(1000);
ADC_INIT();
RD_JESD_INIT();
return 0;
}
Best regards
kailyn