Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4400: AFE4400

Part Number: AFE4400

I am using AFE4400 for getting PPG signals from the artery. W e are getting the attached graph in Arduino ide by using below code (graph and code attached).

Please let me know how can measure PPG signals correctly using Arduino

#include <SPI.h>
#include "protocentral_afe44xx.h"

#define AFE44XX_CS0_PIN   7
#define AFE44XX_CS1_PIN   8
#define AFE44XX_CS2_PIN   9
#define AFE44XX_CS3_PIN   10
#define AFE44XX_CS4_PIN   11
#define AFE44XX_PWDN0_PIN 2
#define AFE44XX_PWDN1_PIN 3
#define AFE44XX_PWDN2_PIN 4
#define AFE44XX_PWDN3_PIN 5
#define AFE44XX_PWDN4_PIN 6
#define AFE44XX_INTNUM    0


AFE44XX afe44xx0(AFE44XX_CS0_PIN, AFE44XX_PWDN0_PIN); 
AFE44XX afe44xx1(AFE44XX_CS1_PIN, AFE44XX_PWDN1_PIN);
AFE44XX afe44xx2(AFE44XX_CS2_PIN, AFE44XX_PWDN2_PIN);
AFE44XX afe44xx3(AFE44XX_CS3_PIN, AFE44XX_PWDN3_PIN);
AFE44XX afe44xx4(AFE44XX_CS4_PIN, AFE44XX_PWDN4_PIN);

afe44xx_data afe44xx_raw_data0;
afe44xx_data afe44xx_raw_data1;
afe44xx_data afe44xx_raw_data2;
afe44xx_data afe44xx_raw_data3;
afe44xx_data afe44xx_raw_data4;

void setup()
{

  Serial.begin(57600);
  Serial.println("Intilaziting AFE44xx.. ");
  
  SPI.begin();
  afe44xx0.afe44xx_init();
  afe44xx1.afe44xx_init();
  afe44xx2.afe44xx_init();
  afe44xx3.afe44xx_init();
  afe44xx4.afe44xx_init();
  Serial.println("Inited...");
}

void loop()
{
  static uint32_t diff = 0,start_time = 0;
  static bool start_flag = 0;

if(start_flag == 0)
{
  start_flag = 1;
  start_time = millis();
}

diff = millis() - start_time;

 if(diff <= 10000)
{
 afe44xx0.get_AFE44XX_Data(&afe44xx_raw_data0);
/////////////////////////////////////////////////    
  Serial.println(afe44xx_raw_data0.RED_data);
  
}  
/////////////////////////////////////////////////
else if(diff >= 10000 && diff <= 20000)
{
  afe44xx1.get_AFE44XX_Data(&afe44xx_raw_data1);
/////////////////////////////////////////////////
  Serial.println(afe44xx_raw_data1.RED_data); 
}
/////////////////////////////////////////////////
//else if(diff >= 20000 && diff <= 30000)
//{
 // afe44xx2.get_AFE44XX_Data(&afe44xx_raw_data2);
/////////////////////////////////////////////////   
 // Serial.println(afe44xx_raw_data2.RED_data);
//}  
//else if(diff >= 30000 && diff <= 40000)
//{
/////////////////////////////////////////////////
 // afe44xx3.get_AFE44XX_Data(&afe44xx_raw_data3);
/////////////////////////////////////////////////  
 // Serial.println(afe44xx_raw_data3.RED_data);
//}  
/////////////////////////////////////////////////
//else if(diff >= 40000 && diff <= 50000)
//{
 // afe44xx4.get_AFE44XX_Data(&afe44xx_raw_data4);
/////////////////////////////////////////////////
 // Serial.println(afe44xx_raw_data4.RED_data);
//}  
else if(diff >= 20000)
{
  start_flag = 0;
}

/////////////////////////////////////////////////
 // Serial.println(afe44xx_raw_data0.IR_data);
/////////////////////////////////////////////////
 // Serial.println(afe44xx_raw_data1.IR_data);
/////////////////////////////////////////////////
 // Serial.println(afe44xx_raw_data2.IR_data);
/////////////////////////////////////////////////
 // Serial.println(afe44xx_raw_data3.IR_data);
/////////////////////////////////////////////////
 // Serial.println(afe44xx_raw_data4.IR_data);
/////////////////////////////////////////////////
 delay(8); 
}

  • Hello Apakrita,

    You will need to read out data based on the ADC_RDY interrupt from the AFE instead of the Arduino based timer.

    Also check with the Arduino driver code owner for more details. TI doesn't own this code to offer any comments on the data.