Part Number: ADS1158
Dear TI forum,
I have 3 x ADS1158 on a shared SPI bus. Let's call them ADC A, B and C. I am using 2 GPIOs for toggling a MUX in order to properly set the chip select pins for each ADC. The MUX is SNx4HC139. Each DRDY pins are connected to 3x GPIOs, one for each ADC. Both ADC A and B are configured identically (let's ignore ADC C for now):
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] ADC 0 reset.
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] ADC 1 reset.
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] ADCs configured succesfully. ADCs configuration:
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] Register 0x0 Value 0x5e
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] Register 0x1 Value 0x31
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] Register 0x2 Value 0x0
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] Register 0x3 Value 0xf
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] Register 0x4 Value 0x0
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] Register 0x5 Value 0x0
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] Register 0x6 Value 0x0
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] Register 0x7 Value 0x7f
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] Register 0x8 Value 0x0
Nov 28 13:21:42 raspberrypi acquisition[163587]: [INFO] Register 0x9 Value 0x9b
I am trying to sample the ADCs in the following sequence (I will ignore ADC C for simplicity below):
1. Toggle MUX to select ADC A.
2. Send start sampling pulse to ADC A (see code below).
3. Toggle MUX to select ADC B.
4. Send start sampling pulse to ADC B.
5. Toggle MUX to select ADC A.
6. Poll its DRDY gpio and if it becomes 0 then read data from ADC A with Channel Data Read Command (see code below).
7. Toggle MUX to select ADC B.
8. Poll its DRDY gpio and if it becomes 0 then tead data from ADC B with Channel Data Read Command.
Start sampling pulse:
char pulse = 0b10000000;
spi_send(handle, &pulse, NULL, sizeof(pulse));
Channel Data Read Command:
char tx[] = { 0b00110000, 0x00, 0x00, 0x00 };
spi_send(handle, tx, rx, sizeof(tx));
The whole read channel command with timeout:
bool adc_read_channel(int ready, int handle, char* rx) {
uint8_t gpio = 0;
uint32_t start = gpioTick();
uint32_t current = gpioTick();
int diff = current - start;
while (gpio == 1 && diff < TIMEOUT) {
gpio = gpioRead(ready);
current = gpioTick();
diff = current - start;
}
if (diff >= TIMEOUT) {
return false;
}
// Read sample
char tx[] = { 0b00110000, 0x00, 0x00, 0x00 };
spi_send(handle, tx, rx, sizeof(tx));
return true;
}
Very often I get a timeout on ADC B (meaning its DRDY pin does not go low within 100ms or something resets it while handling SPI transfers for ADC A). I've added some logs:
Nov 28 13:13:52 raspberrypi acquisition[162518]: [INFO] adc a channel 0 start sampling drdy a 1 b 1 c 1 cs 0 cs 1 (mux 0b01 selects ADC A)
Nov 28 13:13:52 raspberrypi acquisition[162518]: [INFO] adc b channel 0 start sampling drdy a 1 b 1 c 1 cs 0 cs 0 (mux 0b00 selects ADC B)
Nov 28 13:13:52 raspberrypi acquisition[162518]: [INFO] before channel read drdy a 0 b 1 c 1 cs 0 cs 1
Nov 28 13:13:52 raspberrypi acquisition[162518]: [INFO] after channel read drdy a 1 b 1 c 1 cs 0 cs 1 (DRDY for ADC A toggles from low to high, as expected)
Nov 28 13:13:52 raspberrypi acquisition[162518]: [ERROR] adc timeout on DRDY pin 26 gpio value (active low) 1 diff 100000 (100ms).
Nov 28 13:13:52 raspberrypi acquisition[162518]: [ERROR] drdy a 1 b 1 c 1 (DRDY pin for ADC B never toggled during the while loop)
Nov 28 13:13:52 raspberrypi acquisition[162518]: [ERROR] cs 1 0 cs 2 0 (mux selected 0b00 ADC B)
It works ok for ADC A but DRDY from ADC B was not detected to go low. Or maybe it went low and then high again before getting to that loop but I'm not so sure what could possibly reset DRDY.
Questions:
1. Does DRDY reset when SCLK runs for another ADC even though its CS is high? It's a shared SPI SCLK and datasheet says that DRDY goes back high on the first falling edge of the SCLK.
2. Could ADC B also get the commands from ADC A and react on those even though its CS is high?
3. Sometimes it works, sometimes it doesn't. It works if I add some artificial delays here and there but it's not consistent. What else could cause DRDY to reset?
4. Should I completely ignore DRDY and rely only on the NEW bit from the STATUS byte?
Many thanks!