Part Number: DAC7574
Hi,
We are using DAC7574 for voltage margining RAA2142504GSP#HA0. Kindly help us to calculate the RDAC value in Voltage DAC. What value needs to be used for VDAC and RSET.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC7574
Hi,
We are using DAC7574 for voltage margining RAA2142504GSP#HA0. Kindly help us to calculate the RDAC value in Voltage DAC. What value needs to be used for VDAC and RSET.
Hello,
I would need more details to help support this request. What is the desired output range of the RAA2142504GSP#HA0? Do you already have resistors selected for R1 & R2? Is the below figure a good representation on how you plan to connect the DAC to the circuit?

Best,
Katlynne Jones
Hi Jones,
Desired output voltage 3.3V, we have selected resistors R1=97.6K, R2=57.6K. Yes the representation you mentioned is correct. We will be using like this.
We need R3 resistor value for margining the voltage of 10%. Help us to calculate the value.
Thanks,
S Sathya shree
Hello,
Thanks for the additional information. Based on the RAA2142504GSP#HA0 reference voltage of 1.224V, you can use a R3 resistor of 348kΩ with a VDAC,low of 47mV (DAC code 0x5) and VDAC, high of 2.4V (DAC code 0xFDC0) to margin by 10%. VDAC,low corresponds to a 3.63V output and VDAC,high corresponds o a 2.97V output.
We do have a calculator tool available on ti.com to help with this calculation.
https://www.ti.com/tool/download/VOLTAGE-MARGINING-CALCULATOR
I'm attaching a version that uses the values you shared. If you need to make any modifications to the resistor values in the future you can check with the calculator tool. SmartDAC-Voltage-Margining-Calculator.xlsx
Best,
Katlynne Jones