Part Number: DAC121S101QML-SP
Other Parts Discussed in Thread: LMP7704-SP
Hello, for a current design we are using the DAC121S101QML-SP. Now we need to provide an output current of up to 20mA. The signal is then transmitted via a harness of 1m. At the sensor side there is a load capacitance of up to 10uF.
Do you have any suggestion for a buffer component?
Using an op-amp might end up in oscillation do to the capacitive load.
Best regards
Markus