Other Parts Discussed in Thread: ADS1261
Hi,
I recently started this discussion, but thought I should make another thread as the original question there was answered.
If the REFOUT pin on the ADS1261 is supplying close to the current limit (say 8mA out of 10mA), will that compromise the ADC accuracy at all? I'm aware that the 2.5V voltage will droop by ~400uV, but will the accuracy fall outside the typical room temperature max of 0.2% as the 10mA is reached?
Thanks,
Drew