This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5401-Q1: Questions about DCLK in AFE5401

Part Number: AFE5401-Q1

hi. I have a question about DCLK of AFE5401.

Is DCLK is unconditionally output when a clock is input to the chip?

I'm inputting 25 MHz clock into the chip, but dclk is outputting 3.3v and the waveform doesn't occur.

I would appreciate it if you could let me know the conditions under which dclk can be output.

I'm sorry for the rudimentary question. thank you.