Other Parts Discussed in Thread: AMC1311
Hi,
I plan to use the AMC3311 in one of our application.
I would like to connect the two outputs OUTP and OUTN to a single ended ADC input each.
The two single ended ADC inputs can be sampled simultaneously. Difference is calculated in the software.
Each of the two ADC inputs will have a capacitor in the range of 1 to 10nF to GND.
Between the OUTP (of the AMC1311) and the ADC input as well as between the OUTN and the other ADC input I will use a resistor each (to isolate output from the capacitor).
Are there any information on how the AMC1311 can drive capacitive loads? Or how low those isolator resistors can be (so the AMC1311 outputs are still stable)?
Thanks and best regards,
Patrick