This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8588S: REFSEL detection circuit works abnormal without 3.3VDD

Part Number: ADS8588S


Hi Team,

my customer is using ADS8588 and found REFSEL detection circuit works abnormal without 3.3VDD.

Here is the test condition:

1. with 5VDD power up and REFSEL pull down, 3.3VDD is zero,  the internal reference should be disabled while test result shows 2.5V on REFOUT.(See picture1)

2. with 3.3VDD power up, the test shows REFOUT discharge slowly(see picture2), which means internal reference is disabled and REFSEL works as expected.

Could you help to check:

1. Does REFSEL detection circuit need 3.3VDD to work?

2. customer is using external reference(REFSEL pull high), 5VDD and 2.5V external refence power up first,  before 3.3VDD power up, the REFIN/REFOUT pin may have both internal reference and external reference, is there any issue?

Regrards,

Stone