Part Number: ADS8332EVMV2-PDK
Other Parts Discussed in Thread: ADS8332
Hi,
I tried to use the evaluation board of ADS8332 to see the performance, and I saw something that I didn't fully understand.
I injected the following sine wave to the evaluation board:
around 2.5V peak to peak, 1 KHz sine wave (attached a screenshot from the scope).
I configured the GUI to 300KSPS.
the second attached picture is the 1KHz signal that we can see at the GUI:
I was expecting to see around 300 samples per single period of the sine wave, but I see around 40 samples.
also, when I change the sample rate at the GUI, it doesn't really affecting the signal that I see at the GUI.
would you please advise?
thank you very much!