お世話になります。
DAC7311IDCKR 以下項目の仕様上のMAX値をご教示ください。
①Offset error drift
②Gain temp coefficient
③DAC output noise
以上になります。何卒よろしくお願い致します。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kuroda-san,
We usually do not characterize beyond the typical spec in the datasheet, but here is a rough estimation of the max specs:
1) Offset Error Drift = 18 μV/°C
2) Gain Temp Coefficient:
AVDD = 5 V: ±3 ppm of FSR/°C
AVDD = 2.0 V: ±4.5 ppm of FSR/°C
3) DAC Output Noise = 18 μVPP
Thank you,
Erin