Dear Sir ,
Could you please help to support the souce code of the AFE5818 that developed by FPGA via TSW140X, I searched the e2e , but all of the link is failed to open or access, hope for your response asap, thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Source code for TSW140x FPGA was developed by third party hence sorry to inform that original project files are not available.
Thanks!
Regards,
Shabbir
You shall refer to below document:
Reference material for LVDS capture
Regards,
Shabbir
Hi King,
Do you have access to EVM and GUI for AFE5818 and AFE5832? If you have installed these GUIs, then, the SPI config files for quick-start modes would be available in the below locations -
AFE5818 - C:\Program Files (x86)\Texas Instruments\HMC-DAQ GUI\Scripts\AFE5818\QUICK_START\
AFE5832 - C:\Program Files (x86)\Texas Instruments\AFE5832 EVM\Config Files\AFE5832\AFE5832vA\Scripts\Quick Start
You can refer to these scripts for the SPI configuration.
Thanks,
Karthik